9/15/2014 8:03 AM | |
Posts: 57 Rating:
|
Hi all.. i would like to ask about the scada and s7-1200. currently, i'm using Integraxor scada and CPU 1212c. in my situation, my PLC will be at a river in order to monitor the water level. my scada will be a the control centre. both of them will use the GSM modem that support the port forwading. during the demo, i set the PLC ip : 192.168.0.5 scada ip : 192.168.0.33 both of them using the same network. on the scada, it will read the PLC tags using port 102. it work perfectly. now, i need to separate them and using the internet. PLC WAN ip : 183.171.208.194 Scada WAN ip : 183.171.208.195 i already set the port forwarding in GSM modem. and the scada need to read the PLC tags using 183.171.208.194:102 but i failed to connect it. it said the port is not opened. AttachmentSiemens port.zip (50 Downloads) |
Follow us on