5/12/2014 8:13 AM | |
Joined: 7/8/2008 Last visit: 4/6/2025 Posts: 51 Rating:
|
Dear all participants and experts, i got a sinamics G150 cabinet unit with CU320-2DP on it. from the starter software i can found that the CU320 -2 dp assigned as drive object number 1, the vector power unit as drive number 2, and the TM31 drive object number is 3 below is some question from me: 1. i need to access some parameter acyclically by using SFC59/58 from my S7317-2PNDP PLC. from the attached manual, i have to fill the "AXIS" value on the "request header" section. my question is : how should i fill up this "AXIS " Value? what does "AXIS" value belongs to ? 2. few days ago, i do also monitor the r37parameter from AOP display, there i found that each drive object has the same parameter (r 37). if i only want to access the r37 for the Power unit acyclically, what should i do? since i didnt see any index on r37, but founded each drive object has the same parameter. i look forward to your another kind help and information, AttachmentG150_functionManual_chapter6.pdf (166 Downloads) |
Follow us on