3/4/2015 8:28 AM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
Hello experts! This might be somewhat out of topic, but can you please tell me how the addressing works on Step 7 and PCS7? So for instance the DP Slave having 32 bytes consistent which has been addressed (in HWConfig) I 256 onwards which I want to put in DB1 would it be like (as the help function seems to tell): LADDER: W#16#100 or IW256 (or are they the same?) RECORD: P#DB1.dbx0,0 byte 32 ? My actual situation is, I have to integrate a Schenck DP Slave and I'm sent a GSD file that has the name "DISOCONT MASTER (PCI)" which has 2 slots for input and output which both has same lenght (eg "Module 32 bytes consistent"). Thanks for any help!
------------- |
Last edited by: Min_Moderator at: 3/4/2015 1:40:31 PMNew subject after splitting |
|