10/28/2021 10:14 AM | |
Joined: 8/25/2021 Last visit: 7/15/2022 Posts: 11 Rating: (0) |
Hello, I have connected the Internet with a 4G SIM card on my IOT2050, following this, and successfully ping "www.google.com". And with the command "ip a" I have checked the IP address in the ppp item. Then I tried to access the IOT2050 from my PC with this IP address, but it failed. Should I modify some port settings? How can I access the IOT through the 4G net? (like that I used to access it with"192.168.200.1") Best regards! |
Follow us on