Industry Online Support
Technical Forum
5/14/2010 9:01 AM | |
Posts: 159 Rating: (3) |
If you want to use two clients, you have to add an server as well. So what you want to end up with is 3 new Simatic PC stations: 1 ES/OS client (new, WinCC application client) 1 OS server (new, WinCC application) 1 OS client (new, WinCC application client) Now you have two working clients and a server, and an ES. The ES is used as ES and as one of the two Clients. You have to split your OS project into multiuser (in wincc). You have to add an OS Server Simatic PC station (wincc application) and cutnpaste the original "OS project object" from the ES/OS into the newly created OS Server wincc application. You have to insert two Simatic PC stations (WinCC application clients) Search for and read the "Compendium A" for further info on setting up Simatic PC stations. Read this post: Singleuser-->multiuser |
6/2/2011 8:47 AM | |
Posts: 691 Rating: (37) |
Hey Irfan Quadri Since your client won't allow you to shutdown/De-activate the ES/OS; you can manually configure the new OS as OS Client of ES/OS. Create a client project in the New PC as a OS Client , and assign the Server path(\\ ES\............) for the new Client. Keep in mind. This will stop functioning when the ES/OS is deactivated |
Follow us on