2/8/2013 11:20 AM | |
Joined: 3/14/2008 Last visit: 3/14/2025 Posts: 2175 Rating:
|
You can use the function: Link a prototype to a structure or rename an existing link. This function is listed under Standard Dynamics in the Dynamic Wizard. A few tips.... First create the dynamic dialog functionality....Use the following name-> .variablename So no suffix, only the dot and variable name After completion, use the function and select the structure of the custom block you created. After executing the function, the .variablename is changed to the correct structure of the custom block. Good luck |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on