Industry Online Support
Technical Forum
9/16/2010 7:29 AM | |
Posts: 2348 Rating: (264) |
S7-300 (produced after 2002) have MMC, so data in DBs is retentitive, i.e. it would be restored in case of power fault. You don't need anything. |
9/16/2010 4:16 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating: (11) |
Ruca, Be careful not to download the offline DB to plc otherwise you are going to lose the set points. In case you have to change the offline DB later on, save the parameters from online code and change the DB after that not to lose any parameter which is saved in the DB. Regards, Behnam www.sigmaprocess.ca/blog |
Follow us on