8/7/2024 11:49 PM | |
Joined: 7/5/2023 Last visit: 12/4/2024 Posts: 16 Rating: (0) |
Hello, I am trying to backup existing image to USB drive but my disk space is full at 15GB. The backup is failing saying no disk space left on the device is there a way to clean up the disk space so I can perform the backup? Any Suggestions? Thanks. |
8/8/2024 10:52 PM | |
Joined: 7/5/2023 Last visit: 12/4/2024 Posts: 16 Rating: (0) |
Hi, I am using the following command to perform the backup: dd if=/dev/sda status=progress | bzip2 > /media/usb/image.bz2 Once the backup is perform I am trying to boot from USB and restore the image to another IOT 2050 advanced I am not seeing the blue screen once I reboot it skips it goes to existing image on emmc. Can someone guide me in the right direction? Thanks. |
Follow us on