6/7/2011 11:50 AM | |
Posts: 119 Rating:
|
The cpu 315 on which i am working is not communicating with PG so that i can not back up the program.how can i do this??? |
6/7/2011 1:18 PM | |
Joined: 1/28/2009 Last visit: 3/8/2025 Posts: 6860 Rating:
|
Please check the following tpics: Complete procedure of Uploading PLC S7 Project & program from PLC to PG onlineAlso check the simulation module should be activated.When usingMPI connection, it is a common source of error. regards |
6/8/2011 7:51 AM | |
Joined: 5/28/2008 Last visit: 3/17/2025 Posts: 4518 Rating:
|
PC adapter USB(6ES7972-0CB20-0XA0)take its power from the MPI port of the CPU or Profibus if you connected it to profibus.
|
Ayman Elotaify |
|
6/9/2011 8:04 AM | |
Posts: 119 Rating:
|
my cpu is 315 single dp .i think only attached with MPI ....the led was not blinking in the communication adaptor |
Follow us on