12/3/2021 10:13 AM | |
Joined: 10/20/2021 Last visit: 8/24/2023 Posts: 3 Rating: (0) |
Hi! I am a bit new to github and building my own images. How do I build v1.1.1 that work with the current firmware? If I follow the guide on building the example image I get a warning when it is finished (see attachment). ------------------------------------------------------------------------------------------ |
Last edited by: lhvidsten at: 12/03/2021 10:41:26Last edited by: Jen_Moderator at: 12/03/2021 13:00:54New subject after splitting |
|
12/6/2021 9:42 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, You can clone or download the sources of the V1.1.1 release image from here. This should then build the same image which also can be downlaoded as an image file from here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on