5/5/2014 8:20 AM | |
Posts: 1368 Rating:
|
Hello, With PROFINET, only one CPU can be Controller. The other modules (CPU, CP, Et200...) must be devices. So the first thing is, plz update your CP to V1.2 http://support.automation.siemens.com/WW/view/de/49590072 You have a STEP 7 Projekt with3 Stations Station 1: CPU 315 + CP343 Adv(IO COntroller) with a PNIO-System Station 2 and 3: CPU 315 + CP (with activated PN IO Device mode and IP address). Allare compilied. Go to Station 1. In the HW Catalog under PROFINET IO -> I/O -> SIMATIC S7 CPs ->Adv and search the CP343, you use. With Drag&Drop, add the CP to the PN System. Configure the transfer area (Bytes). Compile the STation. Go back to Station2. In the properties of the CP under PROFINET go to coupling. Mark the CP of Station 1 and couple the modules. That it:-) here i found a manual http://support.automation.siemens.com/WW/view/de/30374198/0/en Chapter 7 |
Follow us on