4/9/2009 1:32 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, Abou synchronization - Insert the start-up OBs OB20, OB21 and OB22 into your STEP 5 project. Program the call for FB125 (SYNCHRON), which prompts synchronization between the CPU and the CP, in these OBs. Important for this FB125 is:Interface number (SSNR)
Hope this will helps. Best regards |
4/14/2009 3:40 AM | |
Posts: 3 Rating: (0) |
thanks! UMENCHO, BR |
4/15/2009 9:50 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
The CP1430 can be installed in any PLC slot that is allowed for CP operation (slot label: CP). For your system look at S5-155H Programmable Controller (CPU 948R / CPU 948RL) (from 31th page). Hope this will helps. Best regards Hristo MIhalev |
Follow us on