7/26/2018 8:31 AM | |
Posts: 14 Rating:
|
Hi! I’m just trying PROFINET for the first time. I have a good experience with Profibus, but an virgin with ProfinetJ I have configured PLS S7-1500 with CM1542. I have configured a ET200S node with some I/O cards. I have tried to assign the ET200S to both PLC and CM I/O system but no success. The main error is “IO device failure – IO device not found”. In advance I have configured correct IP address to ET200S using PST software, so the IP should not be the problem. But I don’t know do I need to load some more configuration direct to the ET200S or it happens as in ProfibusDP there the master have the configuration of the slaves. You see in the attached pictures the online status, Article number Online for the ET200S is “?” like the device can not be discovered, but it is on the net and have a correct IP address. Can some one explain what I need to do to get it working, please! I have shared some more pictures on my Onedrive - of my screen for more information on this link: [snip] AttachmentProfinet.zip (62 Downloads) |
Last edited by: icoto_76 at: 7/26/2018 9:36:31 AMLast edited by: Jen_Moderator at: 7/26/2018 12:15:02 PMRemoved link and added files as an attachment. |
|
Follow us on