Industry Online Support
Technical Forum
9/8/2008 1:42 PM | |
Joined: 4/24/2006 Last visit: 9/29/2023 Posts: 8593 Rating:
|
Dear sm123, Please have a look at this faq: http://support.automation.siemens.com/WW/view/en/22319131 Perhaps it's usefull Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
9/9/2008 12:25 PM | |
Joined: 4/24/2006 Last visit: 9/29/2023 Posts: 8593 Rating:
|
Hi sm123, I think you could use an OPC server on panel. But unfortunately it's only possible using Multi panel See link: http://support.automation.siemens.com/WW/view/en/26129375 Perhaps someone else has an idea. Best regards, Wizard |
9/10/2008 7:01 AM | |
Posts: 6 Rating:
|
Is there any way to read the data of the Report system error at PLC end in any of the Data Block or so? |
5/20/2014 11:35 AM | |
Joined: 4/21/2006 Last visit: 9/21/2023 Posts: 511 Rating:
|
New question was splitted to a new thread: Configure RSE with diagnostics via PROFINET. |
Follow us on