3/22/2019 3:24 AM | |
Joined: 8/9/2013 Last visit: 3/16/2022 Posts: 2 Rating:
|
How to configure two S7-300 and also scada as pc station in Tia V14. Can I do all this in TIA 14? How to configure pc station in TIA 14? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/22/2019 7:21:41 AMNew subject after splitting |
|
3/22/2019 8:09 AM | |
Joined: 7/9/2015 Last visit: 3/14/2025 Posts: 4198 Rating:
|
Hi, yes you can do this, you need Step 7 Professional and WinCC Advanced or Professional for Runtime. Please check this: SIMATIC NET: PC software Commissioning PC Stations - Manual and Quick StartRegards, Towome
|
|
|
3/26/2019 1:14 PM | |
Joined: 8/3/2009 Last visit: 3/14/2025 Posts: 14990 Rating:
|
Hello knauto.user Please give us a little bit more information to your topic. -> Which Scanda System do you use (Siemens or non Siemens? WinCC Advnaced RT or WinCC Professional RT?) -> do you only want to use the Scada in the PC Station or also other Simatic Net Functions like OPC Server or Soft PLC or special CPs? -> do you want to program the S7300 PLCs in the TIA Project or do you only want to use it or communicatoin issues and Work with Step7 Manager in Classic? (Informations) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on