8/2/2008 7:47 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, In this manual : http://support.automation.siemens.com/WW/view/en/12996906 In chapter 8, you will find the technical data of the CPUs For the 315-2DP with order number: 6ES7315-2AG10-0AB0 1st interface Type of interface Integrated: RS485 interface Physics RS 485 Electrically isolated No Interface power supply (15 to 30 VDC) Max. 200 mA Functionality • MPI Yes • PROFIBUS DPNo • Point-to-point connectionNo |
Best regards |
|
Follow us on