7/4/2013 7:12 AM | |
Joined: 2/6/2009 Last visit: 3/26/2025 Posts: 939 Rating:
|
Hi, FOR S7 300 to S7 300/S7 400 Here is the one way to communicate between PLC's having inbuilt Profinet interface.Open Communication Wizard. The Sample Project, Software setup and Manual are in thelink. FOR S7 300/400 to S7 1200 With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols support the S7-1200? SIMATIC S7 S7-1200 Programmable controller(see chapter 10.5 for GET/PUT usage and S7 communication setup). Ethernet Communication: Data Exchange between S7-1200 and S7-300/400 (CE-X18) |
Last edited by: Saravana kumar at: 7/4/2013 7:19 AMLast edited by: Saravana kumar at: 7/4/2013 7:18 AM_______________________________________________________________ |
|
7/6/2013 12:11 PM | |
Posts: 19 Rating:
|
Thank you so much |
2/2/2017 9:20 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by elctro hamad is split to a separate thread with the subject Error when configure s7 -communication between two CPU 300. Best regards |
Follow us on