4/29/2019 12:39 AM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello ifnu fajar P; I doubt that there is a standard answer to such as question in Siemens support. Here is a link to a general project solution to link Amazon Alexa (the logic behind the Echo) and a (non-specified) PLC system, using TCP or UDP transmissions; it might provide hints for your application: http://automation.baldacchino.net/?p=397 If you decide to try it this way, here is a S7-1200 FAQ that could help you. How do you program the TSEND_C and TRCV_C instructions for open user communication over the integrated PROFINET interface of the S7-1200/S7-1500 CPU? https://support.industry.siemens.com/cs/ww/en/view/67196808 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 04/29/2019 00:39:57Last edited by: dchartier at: 04/29/2019 00:40:24 |
|
This contribution was helpful to
1 thankful Users |
7/1/2019 11:22 AM | |
Joined: 6/6/2019 Last visit: 8/9/2024 Posts: 16 Rating:
|
hey i'm using smart relais from ALi now i control 8 relais that in turn are connected to the inputs of the plc |
Follow us on