Industry Online Support
Technical Forum
11/20/2011 10:33 AM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating: (4) |
How to connect analog sensor and analog input in s7-1200 ? see pic Tks
|
11/20/2011 10:41 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
i think that sensor uses communication, rather than analog output. TX, RX are transmit, receive signals. |
11/20/2011 10:55 AM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating: (4) |
tks Sensoruniquely have 0-10 v analog output and this wires |
11/20/2011 11:09 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
Do you have a manual of sensor? which is this sensor ? |
11/20/2011 11:18 AM | |
Joined: 4/30/2011 Last visit: 1/9/2022 Posts: 223 Rating: (4) |
tks bro a little mistake - it have 5th wire - voltage out !!! |
Follow us on