12/20/2019 9:40 AM | |
Joined: 9/9/2014 Last visit: 1/25/2023 Posts: 237 Rating:
|
Hello, First -> What modules have you tested? Notify of the order numbers ... **************** All 1200 series PLCs have high-speed inputs with synchronization. However, for large capabilities usually use high-speed (it all depends on your tasks) modules of a distributed peripheral station from the series ET200SP Read the topics below for your question: and FAQs: SIMATIC S7-1500, ET 200MP, ET 200SP, ET 200AL Counting, measurement and position detection A quick guide to your device (Google to help): ********** Your device should just use the standard SSI interface ... The manual also has a short connection diagram - short connection diagram includ in the manual for the S7-1200 PLC (for synhronyzed input). If you have any questions, ask. No - close the topic and rate) |
Last edited by: Jen_Moderator at: 12/20/2019 11:30:35Optimized link. Best Regards |
|
Follow us on