6/7/2022 4:07 PM | |
Joined: 3/1/2022 Last visit: 9/18/2024 Posts: 5 Rating: (0) |
And i need to know how to wiring from PLC to servo motor (5 VDC), my PLC 24 VDC |
6/7/2022 4:14 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Please don't post multiple for the same problem. |
This contribution was helpful to2 thankful Users |
6/8/2022 6:07 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Motor DC, TIA Portal V16 is published within the conference SIMATIC Technology. Jen_Moderator |
This contribution was helpful to1 thankful Users |
Follow us on