Industry Online Support
Technical Forum
11/3/2014 4:51 AM | |
Posts: 122 Rating:
|
Hello Experts, I would like to move a Memory bit for example M100.0 to a variable in data block which is also a bool. Can any one suggest which instruction should I use to do that. Is there any instruction like MOVE which does a copy function or assignment function for Memory bit, where I do not need to make any intermediate conversion. Just a direct assignment, as it is done in structured text or in higher programming language. I want to know if any thing such available in LAD in TIA portal. Looking forward to hear your response. I here with attach you snap shots with regard to my question in a Zip file. Looking forward to hear your response. With regards Johannes
AttachmentZipFile.zip (74 Downloads) |
11/3/2014 6:02 AM | |
Posts: 5225 Rating:
|
Johannes -Our friend Huggy_d1 answered your question. I wanted to say: thank you for the representing your question in such clear way. |
11/4/2014 6:59 AM | |
Posts: 122 Rating:
|
Thank you. |
Follow us on