2/6/2018 9:02 AM | |
Joined: 8/25/2014 Last visit: 5/30/2023 Posts: 123 Rating:
|
Hello all. I have a similar problem with a analog input ON a ET200S unit. I am trying to connect a 2 wire transducer (a 4-20 mA Endress Hauser FMX 21 level measuremet probe) to a analog input. I have a 2 wire and a 4 wire input avaliable. I connected the + of the probe to M+ and the – to M- (see the attached picture) If I connect a 4-20 mA signal generator with it's own power supply to the input the input works. I get a 4-20mA value. I tried to connect the probe to a 4 wire input, but it's the same. Can some one please point me in the right direction how to corectly wire this trasducer to the input so that I get a 4-20mA value. Thank you in advnced. Best regards. Aleix ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/6/2018 2:23:48 PMNew subject after splitting |
|
Follow us on