4/11/2012 10:22 PM | |
Posts: 11 Rating:
|
here is an image of my connectioon and adresses |
4/11/2012 10:27 PM | |
Posts: 11 Rating:
|
Here is one way I am calling SFB48 , I call it in OB1 and in FB2 , I know that I am going to be measuring constantly so OB1 is the block I will use . |
4/11/2012 10:36 PM | |
Posts: 11 Rating:
|
Here is the last way I am doing thius , I am calling SFB48 in FC1 and FC1 is called in OB1 , theres no errors here it seems but still it doesnt work . |
4/13/2012 11:07 AM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating:
|
you need to set SW_GATE |
4/12/2017 8:23 AM | |
Joined: 9/2/2016 Last visit: 8/26/2022 Posts: 1 Rating:
|
Selam I 124.3 VE I 124.4 encoder girişi #w768 ile nasıl ilişkilendirmem gerekir. teşekkürler |
4/12/2017 2:11 PM | |
Joined: 9/27/2006 Last visit: 7/26/2024 Posts: 12270 Rating:
|
Translation from the Turkish text (from Google Translate):
Merhaba Karakedi; Bu forum, İngilizce'yi uluslararası bir dil olarak kullanmaktadır çünkü üyeler birçok ülkeden geliyor ve hepsi aynı deyi konuşmuyor. Lütfen forumda bir sonraki gelişinizde sorularınızı İngilizce olarak tercüme etmeye çalışın (şu an Google Translate'i kullanıyorum, böylece ne kadar iyi çalıştığına karar verebilirsiniz). Hello Karakedi; This forum uses English as an international language, since members come from many countries and do not all speak the same idiom. Please try to translate your questions in English (I am using Google Translate right now, so you can judge how well it works) next time you come to the forum. If your CPU supports the technological function "Counting" (a CPU 31xC will be able to use its integrated digital inputs to do so) and the encoder is an incremental one (it produces pulses that the CPU can count), then look at the follwing documents and sample programs: SIMATIC S7-300 CPU 31xC Technological Functions See chapter « Counting, Frequency Measurement… » Sample programs for CPU 31xC Technological Functions V1.0 SIMATIC S7-300 Getting Started - Commissioning a CPU 31xC: Counting Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/12/2017 2:58:27 PMLast edited by: dchartier at: 4/12/2017 3:31:57 PM |
|
Follow us on