3/29/2022 2:57 PM | |
Joined: 2/7/2022 Last visit: 6/30/2022 Posts: 4 Rating:
|
Hello, I am quite new in Siemens plc, TIA portal and simatic panel. Currently for my project, I am using Siemens TIA portal, controller - Simatic ET200 CPU, and HMI - KTP700F Mobile Simatic Panel. For my project I am trying to save a csv file in USB flash drive which is attached to my HMI panel so that I can read/write data in HMI. To do that I have used VB script in siemens TIA portal. So far I have used following codes but nothing worked in my case. [snip] Can anyone please suggest my what am I missing or what I need to do actually? I am quite new and I am totally blank in this case. Right now I have exisiting plc project but I don't need to read/write value from my plc project data. I just need to create a simple csv file which can be loaded in USB flash drive and with the internal tag in HMI, I will be able to read/write data in HMI from the csv file. Thanks in advance. AttachmentCoding.txt (496 Downloads) |
Last edited by: Showmik74 at: 03/29/2022 14:59:19Last edited by: Jen_Moderator at: 03/30/2022 09:15:12Added code as a txt file. |
|
Follow us on