7/25/2018 9:09 AM | |
Joined: 4/28/2015 Last visit: 1/25/2023 Posts: 385 Rating:
|
Hello, use the Technology Object (TO) "PositioningAxis" of the SIMATIC S7-1200... If your stepper motor drives uses 24V data signal, you could connect directly to the controller, if you need 5V data signal, you have to use a Signal Board, like SB1222 (6ES7222-1AD30-0XB0) with only DQ or SB1223 (6ES7223-3AD30-0XB0) with DI and DQ. For more information, see manual in chapter 10.3.and following... Or have a look to the following FAQ of TIA V11, but it is the same principle now in TIA V15: Which Motion Control functions are there in STEP 7 (TIA Portal) V11 and how do you use these functions? |
7/25/2018 10:53 AM | |
Posts: 10 Rating:
|
stepper drive use the 24 V signal. I have a wiring diagram for PLC and drive, but I am not sure, can you correct it? Attachmentwiring.pdf (165 Downloads) |
Follow us on