4/25/2016 12:47 PM | |
Joined: 12/7/2009 Last visit: 10/1/2023 Posts: 32 Rating:
|
Hi, How to add text to Textlist in_Faceplates_(Context WinCC V13 Comfort.) Here I could create textlists but can't select individual text list & add rows specific to particular textlist. The same texts are displayed in all textlists. Say if I want to create Text_List_1 is Current, Voltage, Power etc.. & Text_List_2 is Temperature, Pressure, Flow etc.. I couldn't do this in a faceplate. Instead if I add Current, Voltage, Power etc.. in Text_List_1, the Texts in middle section is same for all text lists. When used in project only Text_List_1 works & rest of them doesn't even display the wrongly assigned text. How to Create them!? Thank you. AttachmentText List Faceplate.zip (307 Downloads) |
Follow us on