Industry Online Support
Technical Forum
6/20/2007 5:13 PM | |
Posts: 86 Rating: (2) |
Hello!, I amnew to usingWin CC 6.2. I have started a new project under D:\tst3 folder. However when I try to set the Graphics Runtime Tab in the Computer menu the Path file shown is default (\\COMP2\WinCC60_Project_TST3\TST3.mcp) I am not able to edit this. So my start picture & toolbar menu are empty as the graphics are stored in D drive folder. I am also not able to go to runtime mode as it is asking for start picture. Any suggestions? Thanks, Techy |
6/20/2007 11:12 PM | |
Posts: 17 Rating: (2) |
Have you installed patch for WinCC6.2.. |
6/23/2007 7:38 AM | |
Posts: 86 Rating: (2) |
Hello, Thanks everyone. I got it running. Regards, Techy |
6/25/2007 1:30 PM | |
Posts: 1275 Rating: (123)
|
You're welcome. Good to hear that! |
Follow us on