6/7/2011 5:24 PM | |
Posts: 13 Rating:
|
Dear Experts. For a row of quality tests i need to create a lot of different Step7/NCM hardware configurations. I try to use the command interface to automate the creation of the configs. [schnippschnapp]How to edit the device-specific parameters of a Profibus DP Slave? (Note: Using HWConfig program these parameters can be altered by opening the properties of the according ProfibusDP Slave and switching to “parameters” in the header of the properties window. Find attached a german example picture) I used the following code: [code] 'Auslesen der Gerätespezifischen Parameter 'Ändern der Gerätespezifischen Parameter Splitted from Command-Interface - How to use ProfibusDP Slave Parameters?. |
Last edited by: O_Moderator at: 6/9/2011 12:50 PMnew subject after splitting Last edited by: Applicant at: 08.06.2011 17:06 |
|
Follow us on