8/9/2017 2:34 PM | |
Posts: 19 Rating: (0) |
Hello, regards AttachmentInstallation_ExPC_OG_de_en.pdf (353 Downloads) |
8/17/2017 9:32 AM | |
Joined: 10/18/2012 Last visit: 8/21/2024 Posts: 225 Rating: (23) |
Hello Pavel, according to the instruction manual at https://support.industry.siemens.com/cs/ww/en/view/109741589 this MLFB indicates Windows Embedded 7 as Operating System and capacitive Touch TFT. If your display is Multitouch capable and your Operating system is Windows Embedded 7 (WS7E), then you must switch your Touch-Screen into Single-Touch mode in order to process the touch events correctly. Otherwise the touch will not work. See https://support.industry.siemens.com/cs/ww/en/view/99919105 for details. License Transfer can be done via USB but is also possible via network interface. Just use the Automation License Manager for that purpose. regards,
|
Follow us on