2/9/2010 2:12 PM | |
Posts: 2 Rating: (0) |
I allready done mapping using the manual ( http://support.automation.siemens.com/WW/view/en/39040038 and its working for the two PLC's but the expansion module inputs and outputs is unable to read and its showing some error. Type A I went for... If i am not configuring the expansion modules its having no error and the communication is solid.. When ever i am trying to configure with the expansion modules then its going to error and i can't read the status of the corresponding input/output modules...... |
Last edited by: O_Moderator at: 9/16/2010 2:31 PMlink edited Last edited by: MathewS at: 2/9/2010 2:44 PMLast edited by: MathewS at: 2/9/2010 2:26 PM |
|
Follow us on