6/7/2012 12:52 PM | |
Joined: 8/31/2010 Last visit: 1/9/2025 Posts: 1523 Rating: (230) |
Hello trapper66, Activate the system events and you will get the 140000 - Connection alarms as shown here If you want life bit of HMI in PLC then for S7-300 / S7-400 - "Coordination" area pointer S7-1200 - Area pointer "Coordination" |
Like it? Rate it! |
|
6/11/2012 3:30 PM | |
Posts: 3037 Rating: (192)
|
Hello, I have found this FAQ for WinCC flexible. You can use this in WinCC V11. How can you visualize the current status of the CPU on a WinCC flexible operator panel? Tweety |
This contribution was helpful to2 thankful Users |
1/22/2018 5:58 PM | |
Posts: 45 Rating: (0) |
Hi guys, I got a problem with this coñNecton. In our setup I had used 2 plc talking to one hmi. In this case if I used this 14000 coñnecation if I loss one plc also this alarm will come. Can I take a bit which is different for these plc connections on hmi Thabks antony
|
Follow us on