8/28/2014 9:54 PM | |
Posts: 5225 Rating: (1184) |
Hi Kahl, Thank you for the feedback. huggy_d1 has already given you some valued ideas. Becuase I am envious of the conversation, I will share my ideas with you too. ( [smile] don't worry.. the above is just try to keep the conversation light.) I use sequencing very much in our designs. Normally I use the bits within a WORD or DWORD as the step indicator. Let assume we have declared STEPS as a DWORD. Then the first step in the sequence is STEPS.x0 (slicing method). The first order of business is to start the sequence cycle.. 1 ------ MOVE ------- STEPS Then next is the conditions which uses a SHIFT instruction.. (conditions) ------------> SHIFT STEPS by 1 Elsewhere I use the STEPS.x# to do the actions. Maybe it works for you.. maybe it does not. To better explain I attach a picture. Note that this is not an acual program but only an idea. Replace condition_# and action_0 with your own (group of) variables. |
Last edited by: William B. at: 8/28/2014 11:11 PMpart 2 follows Last edited by: William B. at: 8/28/2014 9:56 PMformat |
|
This contribution was helpful to1 thankful Users |
Follow us on