10/7/2018 1:41 PM | |
Posts: 1 Rating: (0) |
we have 1000 kw Siemens AC Motor and for each motor we have 2 motor module in parallel, modules are 6SL3320 1TG38 1AA3. There is fault in CU 320, fault no. - F7802, DC Link Voltage is Low. Checked DC link voltage in other drive connected on same DC link is 970 VDC. One of the motor module which are connected parallel has some problem in DC link voltage sensing module because we checked 560 Amp all 8 fuse in both the modules found healthy. How to find that which motor module has problem. Is there any way to connect motor module through Drive cliq.
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/8/2018 2:09:25 PMNew subject after splitting Last edited by: The Helping Hand at: 10/8/2018 2:12:15 PMDeleted personal information |
|
This contribution was helpful to1 thankful Users |
Follow us on