Industry Online Support
Technical Forum
7/9/2010 8:14 AM | |
Posts: 12 Rating: (2) |
Ok, I wrote down the code to implement what I need ( I attach it here...is written in an hurry up, so it is not very good example) but now I 've got another problem: I can't read the Event Text in the OS, for both the alarm_8P and the MSG_NACK. The alarm text message does not show up in the alarm page and the alarm page that belong to faceplate. I've got only the origin ( eg. the chart/blockname). Any idea?
AttachmentMeasMon2WithNack.zip (45 Downloads) |
7/12/2010 8:42 AM | |
Posts: 12 Rating: (2) |
Ok, is anybody is interested, here the final code: it seems to work. If anybody else got other solutions or have suggestions...I think that can be improved, but now I don't have time.AttachmentMeasMon2WithNackFV.zip (68 Downloads) |
This contribution was helpful to2 thankful Users |