9/4/2017 7:44 AM | |
Joined: 12/8/2014 Last visit: 4/15/2022 Posts: 10 Rating:
|
We have installed: Product: Drive ES - Starter setting Installation Path to "C:\PROGRA~2\SIEMENS\Step7\U7umc\data" u7bt05ax.exe -p C:\PROGRA~2\SIEMENS\Step7\U7umc\data succeeded! COM exception: 0x80004005 Unspecified error Microsoft Access Database Engine : could Not make changes because of duplicate values in the index, primary key or relationships. Modify data in one or more fields containing repeating values, delete an index or redefine it to allow duplicate values and try again. SQL statement : INSERT INTO PRODGROUP_VERSIONS (KEY_PGV,VERSION_PGV) VALUES (146,12) u7bt0cax.exe: error: Fehler beim HW-Katalog Import Tell us how to install SSP G120 v4.7 sp6 Error "SQL statement : INSERT INTO PRODGROUP_VERSIONS (KEY_PGV,VERSION_PGV) VALUES (146,12)" occurs when you install SSP G120 V4.7 sp6 for starter 4.4.0.3 such an error does not occur. Then when you restart starter 4.4.1.0 in fact, in the installed devices G120 V4.7 sp6 there, but when inserted into a project G120 V4.7 sp6 in the project nothing is inserted. G120 V4.7 sp3 to the project is inserted. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_393519 at: 9/7/2017 7:54:31 AMLast edited by: Jen_Moderator at: 9/13/2017 8:34:30 AMNew subject after splitting |
|
9/4/2017 7:54 AM | |
Joined: 5/12/2006 Last visit: 2/6/2025 Posts: 22526 Rating:
|
Hello, the SSP 4.7 SP6 is already installed, you don't need to install it again. regards Christoph |
Follow us on