8/3/2007 2:47 PM | |
Posts: 5822 Rating: (412)
|
Dear Swilly, well, a direct Module to be a Master for Allen Bradley is not known to me, but I have some Samples with either Ethernet or Profibus from the Applications & Tools Portal on this page. Communication between SIMATIC S7 and Allen-Bradley ControlLogix CPUs via Ethernet: Use of "Echochange" gateways Communication between SIMATIC S7-CPUs on PROFIBUS and Allen-Bradley Controllers via SST PROFIBUS Scanner Connection between PROFIBUS Networks and DeviceNet by Anybus X-Gateways I hope this will help a bit. Best regards J_Bell |
8/8/2007 11:25 PM | |
Joined: 8/10/2006 Last visit: 8/13/2024 Posts: 298 Rating: (29) |
Jesper, The module is an IM466. I still haven't found the PDF. I'll keep checking. |
8/9/2007 10:32 AM | |
Posts: 5822 Rating: (412)
|
This would never happen... I know it. J_Bell |
Follow us on