2/8/2011 8:55 AM | |
Posts: 173 Rating: (95)
|
Hey Justin Thanks! This is also something that I would like to do. My current problem is how to interface the GSM unit to the LOGO! If the GSM modem only has a 2.8V output, how are you getting it into the LOGO! 24V or 12V DC inputs so that the LOGO! 'sees' it? Any ideas of getting pulses from the LOGO! relay or transistor outputs back to the modem i.e. from 12V / 24V dc down to 2.8V ?!?!?! Thanks Splitted from Select which relay to switch based on number of pulses on a single input. |
Last edited by: O_Moderator at: 2/8/2011 12:00 PMnew subject after splitting |
|
2/8/2011 12:36 PM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715) |
Hello Logo!Barbarian, Don't know your electronic skills, but optocouplers will do the job for you. http://www.jaycar.com.au/images_uploaded/optocoup.pdf hope this helps. |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
2/8/2011 1:24 PM | |
Posts: 2930 Rating: (432)
|
Hi, you can also use the AI to detect 2.8V if you have AI's. Regards Helmut |
This contribution was helpful to1 thankful Users |
Follow us on