8/30/2012 4:14 PM | |
Posts: 2 Rating:
|
I would like to make communication through cable micro-usb, is it possible? If yes how do I setup Opc Server? |
8/30/2012 4:33 PM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Hello Vitors, I think you mean USB-PC Adapter?
Here are some guidelines, (But they do not use USB-PC Adapter) how do you configure an S7 connection for the SIMATIC NET OPC server via PROFIBUS with the SIMATIC NET PC software? how do you configure an S7 connection for a user application via MPI with the SIMATIC NET PC software? how do you configure an S7 connection via MPI with the SIMATIC NET OPC server and the SIMATIC NET PC software? Best regards, Wizard |
12/13/2013 12:46 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question splitted to |
1/29/2014 11:02 PM | |
Joined: 9/1/2005 Last visit: 3/10/2025 Posts: 4113 Rating:
|
follow up question published by LKMNVRSis split to a seperate thread with the subject Connection 9 PLC's to one PC via OPC. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on