1/24/2013 5:56 AM | |
Posts: 241 Rating:
|
hello all I have CP5711-6GK1571-1AA00...it comes without MPI cable. Can anyone help me , how to make MPI cable for this??? |
1/24/2013 8:02 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello Deep, You Can Used the Profibus Cable as Said, or also Normal Shielded Cable, In MPI & Profibus Following Pin are used 3 - Data - (If Profibus Cable Used then Red Cable) 5 - GND 8 - Data + (If Profibus Cable Used then Green Cable) So you can used on ly Pin 3 & 8 in Normal D Type Connector |
Ammy |
|
This contribution was helpful to
1 thankful Users |
Follow us on