12/29/2009 10:47 AM | |
Joined: 9/23/2005 Last visit: 9/27/2023 Posts: 4237 Rating:
|
Hi, That is a difference of names for the same thing PLC UInt = HMI UShort PLC DInt = HMI DShort in the S7-1200 the block "CONVERT" converts Word in UInt or Dword to UDint Attachmentexample.zip (1061 Downloads) |
Last edited by: Pegaia at: 12/29/2009 3:55 PMI change the open file to this one, that converts bool to UInt and vice versa Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
3/18/2010 4:38 PM | |
Joined: 9/23/2005 Last visit: 9/27/2023 Posts: 4237 Rating:
|
Hi, An enhanced version of the open example is available as FAQ in http://support.automation.siemens.com/WW/view/en/41512046 |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
7/17/2016 10:15 PM | |
Posts: 5225 Rating:
|
Hard to be of help without seeing a sample program. Also see if a recent post can be of help.. w |
This contribution was helpful to
1 thankful Users |
11/21/2018 10:59 PM | |
Posts: 1 Rating:
|
https://support.industry.siemens.com/tf/ww/en/posts/siemens-logo-ktp400-hmi-alarm-tags/162174/?page=0&pageSize=10#post661834 |
Follow us on