9/15/2017 12:36 PM | |
Joined: 3/16/2014 Last visit: 10/14/2021 Posts: 120 Rating:
|
Unicode files should use the extension .txt ANSI files should use .csv |
9/19/2017 12:52 PM | |
Joined: 8/3/2009 Last visit: 2/14/2025 Posts: 14758 Rating:
|
Hello Devendra Thakur The Excel Viewer is only able to open Excel files like xls or xlsx. CSV is not an Excel Format!! The only way to oben a csv File on a Comfort panel is to use the Webbrowser but then you will see only the native text of the File without columns formated like in Excel or a csv Viewer. look in the toolbox there is als a solution to readout the csv File again but only with the help of a lot of scrips: https://support.industry.siemens.com/cs/de/en/view/106226404 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on