Industry Online Support
Technical Forum
2/14/2011 10:14 AM | |
Joined: 4/29/2010 Last visit: 12/16/2022 Posts: 1557 Rating:
|
Hello, i have take a look at your screenshot. This isn`t a backup sadly. A backup can be done with ProSave or on a memory card for example: http://support.automation.siemens.com/WW/view/en/28928853 The files at your card are not some backup files, these are just the runtime file and the passwordlist but not the needed project file. If you haven`t got the original project file (ProTool: xxx.PDB ; flexible: xxx.hmi) then you can`t convert the MP370 to a MP377 or migrate the project to from ProTool to WinCC flexible. best regards. |
2/14/2011 11:29 AM | |
Posts: 93 Rating:
|
Thanks a lot for your reply..! |
Follow us on