Industry Online Support
Technical Forum
10/24/2013 4:07 PM | |
Posts: 220 Rating: (11) |
Hi manute Do you switch the connection in PLCSIM and WinCC to the same PLCSIM connection? |
10/24/2013 4:27 PM | |
Posts: 220 Rating: (11) |
And a sacound question: Do you allowed in the "Projekt Properties > Options" in WinCC, the activation of the WinCC Runtime on the ES?
|
10/24/2013 4:28 PM | |
Posts: 29 Rating: (0) |
No, I didn't |
10/24/2013 4:37 PM | |
Posts: 220 Rating: (11) |
Which PCS 7 and WinCC version do you use? |
10/24/2013 4:52 PM | |
Posts: 29 Rating: (0) |
PCS7 v8 upd1 and WinCC 7.0 + sp3 + upd 1 |
10/24/2013 5:33 PM | |
Posts: 220 Rating: (11) |
And should check the Settings"Options > Set PG/PC Interface"in the SIMATIC Manager. With PLCSIM in use the setting have to be "PC Internal".
|