8/22/2011 9:27 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, in this case you have to do a OS-update with the option reset to factory settings. How do you do an operating system update (OS update) on operator panels? best regards |
8/22/2011 10:30 AM | |
Joined: 4/22/2010 Last visit: 1/15/2025 Posts: 5697 Rating:
|
If there are some optional tools on the panel yes, if it's a basic winccflex panel, no. You can read more about licenses here : http://support.automation.siemens.com/WW/view/de/27005215 Regards, Marcjan |
Problem solved? |
|
8/22/2011 10:45 AM | |
Posts: 12 Rating:
|
Hello Marcjan |
8/25/2011 12:14 PM | |
Joined: 4/24/2006 Last visit: 2/18/2025 Posts: 8855 Rating:
|
Dear Mervyn, Here is link to manual: SIMATIC HMI HMI Device TP 177A, TP 177B, OP 177B (WinCC flexible) See chapter 7.5 And 7.5.5, you will need MAC Address. Best regards, Wizard |
Follow us on