11/9/2019 1:10 PM | |
Joined: 9/9/2014 Last visit: 5/21/2024 Posts: 245 Rating: (40) |
Hi All I created the question in this thread, so as not to create another ... I have a similar question, however - about replacing the controller of the same series S7-319-3PN/DP but different versions (different order numbers and firmware versions). There is a topic for replacing PLC: New PLC and install an old flash card on it - will this work? There the question is about replacing without STEP7 However, I tried to perform a replacement inside the program, and saw the message:13:4326 What parameters should I check when replacing (I did not find the answer to this question, maybe I was looking badly ...) I understand that maybe these are network-related settings, usually they are, but what else? Maybe there is some kind of manual on this, can you tell? ------------------------------------------------------------------------------------------ |
Last edited by: Unreality at: 11/11/2019 06:26:51Last edited by: Jen_Moderator at: 11/11/2019 12:50:18New subject after splitting Last edited by: Unreality at: 11/11/2019 12:57:55Last edited by: Unreality at: 12/06/2019 18:00:23Best Regards |
|