9/21/2016 8:02 PM | |
Posts: 11 Rating: (1) |
Dear expert, Can you help me on how to position Sinamics V90 PN from S7 1200. I understand that position control has to be done in the PLC. But when I add a TO in S7 1200, it only allows to configure a PTO drive. How do I configure a Positioning axis in 1200 with V90 PN?? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/23/2016 12:38:34 PMNew subject after splitting |
|
9/24/2016 3:50 AM | |
Joined: 2/25/2014 Last visit: 6/17/2024 Posts: 61 Rating: (4) |
Did you see application example below the link site ?
|
Follow us on