3/8/2013 6:19 AM | |
Posts: 461 Rating:
|
Hi figalamx , As your Printer supports TCP, u can use Tcon,Tsend under the open user communication to establish connection & to send data to the printer.. That's the easiest way, check the below link where u can find the sample program. /tf/WW/en/Posts/46768 Try & revert back if there s any issues. Regards, Nelliyan.G |
3/8/2013 9:09 AM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello figalamx, Have a look at How do you program the TSEND_C and TRCV_C instructions for open user communication over the integrated PROFINET interface of the S7-1200 CPU? This is common for TCP, UDP and also ISO on TCP. |
Like it? Rate it! |
|
Follow us on