9/8/2014 7:02 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello Shreyas, In which PCI slots can you operate the different Industrial Ethernet and PROFIBUS PC CPs? Which SIMATIC NET Industrial Ethernet PC CP is compatible with which Microsoft Windows operating system? you will see the Compatibity, you just need the a Step 7 or WinCC has to be installled, after that if you Installed the CP in PC, it will copy the required Driver from System. |
Ammy |
|
Follow us on