9/19/2017 7:38 AM | |
Joined: 5/15/2010 Last visit: 5/1/2023 Posts: 170 Rating:
|
Hi Experts, It may be strange question from me. I have attached a data sheet, i am getting confused with below queries while reading. Please guide me what to refer for below queries:-
Its clear for me that using one DP master can handle Max 32 slaves, 128 nodes,2048 bytes and max 244 bytes per slave. Correct me if iam wrong. Thanks in advance. Attachment6ES71518AB010AB0_datasheet_en.pdf (41 Downloads) |
9/19/2017 9:15 AM | ||||
Joined: 5/15/2010 Last visit: 5/1/2023 Posts: 170 Rating:
|
Hi mopS04, Thanks for your reply. For point no 2 No. of connectable I/O device means can i connect 128 CPU of same make ? Point 1 and 3 are clear. I have also attached some snapshots of data sheet which needs to be cleared. Also what is
its there in sheet, page 4/13. AttachmentData Sheet.zip (21 Downloads) |
|||
Last edited by: vinit at: 9/19/2017 9:22:04 AM |
||||
9/19/2017 11:20 AM | |
Joined: 5/15/2010 Last visit: 5/1/2023 Posts: 170 Rating:
|
Hi, Thanks for reply. What does Transfer Memory and Submodues indicated in attached file. |
9/19/2017 12:58 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi vinit, when you use the CPU as IO-Device you need to project transfer areas. these can have a maximum of 1440 byte and can be devided in submodules. regards, |
FCK WAR! |
|
Follow us on